Posted on May 17, 2011 at 13:27I can build the application OK using Visual Studio 2008 under Vista, but I get an exception error when trying to run it. The same process works ok under XP Pro. Has anyone experienced the same?
Posted on May 17, 2011 at 13:25watch at your signal impedance going into the adc vs the sample/hold time. It may be that the second conversion occurs when the signal has stabilized further. I've had a few issues with the ADC and its internal capacto...
Posted on May 17, 2011 at 13:18 Thanks for the input. The errata I was able to find talks about a 10ns pulse of 150mV max on ADC0 only. What I see is much longer (almost 5us) and is on every channel with a 30K resistor to ground at the input. ...
Posted on May 17, 2011 at 13:18 I dont know if this is related but I am observing a strange problem at the time a new ADC channel is selected. I am running continuous captures on 12 Channels (including the 2 internal channels vref, temp) with...
Posted on May 17, 2011 at 13:16I see there are version for the str7 and str9. I have not seen any information about code size. Does anyone have these values?