2017-01-04 6:07 PM
Hello, i am new in linux, i am using the STM32 Crypto lib and try to work on the RSA part,
i am using linux command build.
I get the error of
core_cm3.h:136:95: fatal error: core_cmInstr.h: No such file or directory
mInstr.h>and i read this
https://gcc.gnu.org/onlinedocs/cpp/Search-Path.html
i was able to locate the core_cmInstr.h in CMSIS and i have try to more it to the directories as mentioned in the above link.
Can anyone help?
Many thanks~
2017-01-04 7:43 PM
core_cm3.h and core_cmInstr.h should be in the same directory, normally CMSIS/Include
You might want to review the Include Paths and determine where it it is pulling the core file from so you have contemporaneous file versions.
2017-01-04 11:07 PM
Clive One wrote:
core_cm3.h and core_cmInstr.h should be in the same directory, normally CMSIS/Include
You might want to review the Include Paths and determine where it it is pulling the core file from so you have contemporaneous file versions.
yes but the as the include are <> not ''
so this is not work for placing the same directories and
for the latter,
how can i review the the Include Paths and determine where it it is pulling the core file from so you have contemporaneous file versions.?
How can i do the above ?
thanks
2017-01-06 2:12 PM
If you are using GNU/GCC via a makefile you could look at what -I options are being feed into the compiler. If you are using some IDE you'll need to dig into the metadata/option for the project and see where it is defining the C/C++ compiler settings for Include Paths.
In the CMSIS v4.10 both core_cmInstr.h and core_cm3.h reside in the same CMSIS\Include directory, why they would be in different directories on your system, and why it finds one and not the other, would really be a matter for specific analysis of your system, and the build/make process you are using.
2017-01-10 9:28 PM
thanks i have solved the problem.