2018-08-10 10:57 AM
Hello,
i am facing problem with flashing my STM32F769I Disco.
the flashing works when i change to erase full chip instead of sector erase on Keil MDK 5.
Full chip erase takes longer time as usual and i dont prefer full erase every time.
The project is a standard one from keil, refer the attached picture.
kindly let me know proper target settings to use Sector erase(which works when project is generated through cubeMx) for flashing.
2018-08-10 11:36 AM
Load one of the example projects under the HAL/Cube trees, they should build and download without problem. Default setting erase blocks as required.
Anything else plugged into the F769I-DISCO board?
Try a different USB cable, try a different USB port, try a different computer.
Check voltages on the board.
Check current firmware on ST-LINK.
2018-08-26 5:16 AM
hi clive,
-nothing else is plugged into the f769
-yes, i have tried different cables, i mean same cable works for project generated through CubeMx without problems.
-Voltages are stable
-Current ST-Link firmware is up to date .
i seem to be missing some debug or flash settings in target config of Keil. can't figure which one yet.
Could you please try with your setup if you have ? take an example from keil itself and flash.
Thanks.