Skip to main content
RKadl
Associate II
October 24, 2019
Question

Can we use two QUAD SPI of STM32l496RGT separately?

  • October 24, 2019
  • 2 replies
  • 707 views

In our design we use QUAD SPI for memory interfacing, can we use QUAD SPI separately for two different memories.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
October 24, 2019

Yes, should be able to access separately or as a pair.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RKadl
RKadlAuthor
Associate II
October 24, 2019

We trying to interface flash memory on QUAD SPI1 Bank 1, SRAM on another QUAD SPI2 Bank 2. Can it will work?

In application note, QUAD SPI is used for the 4 bit, 8 bit Flash memory interface.