CAN TX not working in normal mode, only Loopback mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-02-20 10:24 AM
CAN TX not working in normal mode, only Loopback mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:25 AM
Hello,
thank you for this hint, the init procedure returns CANINITFAILED. What does this mean? Is the MCU damaged? I bridged the RX and TX (PA11 & PA12), is this okay?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:25 AM
CAN_DeInit stops the clock, so the clock enable has to be done after this command. Now the initialisations works, but when I sent a CAN_Transmit (with RX and TX bridged), the status of the message stays pending, what's wrong now?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:25 AM
Hi mgarza,
From my side i think that your FW configuration is correct. But maybe that you have a HW problem, so what i suggest you to do is to check the return status of CAN_Init(CAN1, &CAN_InitStructure) function (return value must be CANINITOK ) With best regards, HalimFrom: mgarzaPosted: Sunday, February 20, 2011 7:24 PMSubject: CAN TX not working in normal mode, only Loopback modeHello,
I do have the probelem that CAN is not operating in nomal mode, when trying transmit a CAN message the message transmission is not executed. It's working fine in loop back mode, but not in normal mode. I'm using an STM32F103RE microcrontroller. RTS is not used and I get the error when USART1 is switched off. What am I doing wrong? Code RCC init (72MHz): RCC_DeInit(); /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); /* Flash 2 wait state */ FLASH_SetLatency(FLASH_Latency_2); /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* PCLK2 = HCLK */ RCC_PCLK2Config(RCC_HCLK_Div1); /* PCLK1 = HCLK/2 */ RCC_PCLK1Config(RCC_HCLK_Div2); /* PLLCLK = 4MHz * 9 = 36 MHz */ //RCC_PLLConfig(RCC_PLLSource_HSI_Div2, RCC_PLLMul_9); /* PLLCLK = 8MHz * 9 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); /* Enable PLL */ RCC_PLLCmd(ENABLE); /* Wait till PLL is ready */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) {} /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till PLL is used as system clock source */ while(RCC_GetSYSCLKSource() != 0x08) {} CAN init: CAN_InitTypeDef CAN_InitStructure; CAN_FilterInitTypeDef CAN_FilterInitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* CAN1 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_AFIO, ENABLE); // GPIO_PinRemapConfig(GPIO_Remap1_CAN1, DISABLE); // GPIO_PinRemapConfig(GPIO_Remap2_CAN1, DISABLE); GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; /* Configure CAN1 RX pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure CAN1 TX pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Enable the CAN1 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // NVIC_InitStructure.NVIC_IRQChannel = USB_HP_CAN1_TX_IRQn; // NVIC_InitStructure.NVIC_IRQChannelSubPriority = 3; // NVIC_Init(&NVIC_InitStructure); /* CAN register init */ CAN_DeInit(CAN1); CAN_StructInit(&CAN_InitStructure); /* CAN1 cell init */ CAN_InitStructure.CAN_TTCM = DISABLE; CAN_InitStructure.CAN_ABOM = DISABLE; CAN_InitStructure.CAN_AWUM = DISABLE; CAN_InitStructure.CAN_NART = DISABLE; CAN_InitStructure.CAN_RFLM = DISABLE; CAN_InitStructure.CAN_TXFP = DISABLE; CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;//CAN_Mode_LoopBack CAN_Mode_Normal CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; CAN_InitStructure.CAN_BS1 = CAN_BS1_12tq; CAN_InitStructure.CAN_BS2 = CAN_BS2_5tq; CAN_InitStructure.CAN_Prescaler = 4; CAN_Init(CAN1, &CAN_InitStructure); /* CAN1 filter init */ CAN_FilterInitStructure.CAN_FilterNumber = 0; CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask; CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit; CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0; CAN_FilterInitStructure.CAN_FilterActivation = ENABLE; CAN_FilterInit(&CAN_FilterInitStructure); // CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); CAN_ITConfig(CAN1, CAN_IT_FMP0 | CAN_IT_FF0 | CAN_IT_FOV0, ENABLE); // fifo0?? // CAN_ITConfig(CAN1, CAN_IT_TME, DISABLE); // ???? CAN_ITConfig(CAN1, CAN_IT_EWG | CAN_IT_EPV | CAN_IT_BOF | CAN_IT_LEC | CAN_IT_ERR | CAN_IT_WKU | CAN_IT_SLK, ENABLE); // ERR?? CAN Message Transmission (TX): CanTxMsg TxMessage; uint8_t TransmitMailbox = 0; uint8_t i; /* transmit */ TxMessage.StdId=0x123; TxMessage.ExtId=0x01; TxMessage.RTR=CAN_RTR_DATA; TxMessage.IDE=CAN_ID_STD; TxMessage.DLC=1; TxMessage.Data[0]=0x40; TxMessage.Data[1]=0x02; TxMessage.Data[2]=0x1a; TxMessage.Data[3]=0x80; TransmitMailbox = CAN_Transmit(CAN1, &TxMessage);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:25 AM
Just make sure that you have another CAN device with the right baud rate on the network that can receive your packet.
Also you can check the CAN error(CAN_ESR) status register to find out the type of error.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:25 AM
Now I connected 2 MCUs and and uploaded the can_init procedure. Unfortunately the reception of the transmitted data fails, when debuging the can registers of the receiving device I see that the 1st device tries to transmitt the message, but the second reports sometimes ''form error'' and sometimes ''stuff error''.
What's wrong now? Where do I have to searcg for the error now?