CAN Transmit timeout error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-27 9:54 AM
Hi everyone, I�m using a STM32F103 with SW4STM32 and CubeMX and I`m struggeling with the CAN Communication. When I`ll try to transmit Data with HAL_CAN_Transmit then I get a timeout error. Like I read here in other threads it could be a bug from the HAL library but I dont`t know how to solve this problem. Or it could be a problem with my code. So I hope someone can help me.
Here is my code. If you need some other parts of it I`ll post it too.
Thanks for your support
int main(void)
{/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* Configure the system clock */
SystemClock_Config();/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_SPI1_Init(); MX_USART1_UART_Init(); MX_CAN_Init();/* USER CODE BEGIN 2 */
__HAL_UART_ENABLE_IT(&huart1, UART_IT_RXNE);/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ HAL_GPIO_WritePin(GPIOD, USBEnable_Pin, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOD, canRS_Pin, GPIO_PIN_SET); HAL_UART_Receive_IT(&huart1,&Rx_data, 1); printf('welcome\r\n');uint16_t SOC = 5500;
uint16_t BatVoltage = 590; uint16_t cellVoltageMax = 3900; uint16_t cellVoltageMin = 3800; uint8_t tempMax = 50; uint8_t tempMin = 47;while (1)
{ printf('Test\r\n');hcan.pTxMsg->Data[0] = 0b01110000;
hcan.pTxMsg->Data[1] = (uint8_t) (SOC/1000); hcan.pTxMsg->Data[2] = (uint8_t) ((BatVoltage & 0b111111111111) >> 4); hcan.pTxMsg->Data[3] = (uint8_t) (((BatVoltage << 12) | ((cellVoltageMax & 0b0001111000000000) >> 1)) >> 8); hcan.pTxMsg->Data[4] = (uint8_t) (((cellVoltageMax & 0b0000000111110000) >> 1) | ((cellVoltageMin & 0b0001110000000000) >> 10)); hcan.pTxMsg->Data[5] = (uint8_t) (((cellVoltageMin & 0b0000001111110000) >> 2) | (tempMax >> 6)); hcan.pTxMsg->Data[6] = (uint8_t) ((tempMax << 2) | (tempMin >> 6)); hcan.pTxMsg->Data[7] = (uint8_t) (tempMin << 2);printf('Data[0]: %d\r\n', hcan.pTxMsg->Data[0]);
if (HAL_CAN_Transmit(&hcan, 10) != HAL_OK)
{ /* Transmition Error */ //Error_Handler(); printf('CAN Transmit Error\r\n'); } printf('%d\r\n', HAL_CAN_GetState(&hcan)); HAL_Delay(1000); /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */}
/** System Clock Configuration
*/void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{ Error_Handler(); }HAL_RCC_MCOConfig(RCC_MCO, RCC_MCO1SOURCE_PLLCLK, RCC_MCODIV_1);
/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}/* CAN init function */
static void MX_CAN_Init(void){ CAN_FilterConfTypeDef sFilterConfig; static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage;hcan.Instance = CAN1;
hcan.pTxMsg = &TxMessage; hcan.pRxMsg = &RxMessage;hcan.Init.Prescaler = 4;
hcan.Init.Mode = CAN_MODE_NORMAL; hcan.Init.SJW = CAN_SJW_2TQ; hcan.Init.BS1 = CAN_BS1_12TQ; hcan.Init.BS2 = CAN_BS2_5TQ; hcan.Init.TTCM = DISABLE; hcan.Init.ABOM = ENABLE; hcan.Init.AWUM = ENABLE; hcan.Init.NART = DISABLE; hcan.Init.RFLM = DISABLE; hcan.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan) != HAL_OK) { Error_Handler(); }sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 14;if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{ /* Filter configuration Error */ Error_Handler(); }hcan.pTxMsg->StdId = 0x100;
hcan.pTxMsg->ExtId = 0x0; hcan.pTxMsg->RTR = CAN_RTR_DATA; hcan.pTxMsg->IDE = CAN_ID_STD; hcan.pTxMsg->DLC = 8;}
#can-timeout #can #stm32f103- Labels:
-
CAN
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-02 6:37 PM
?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-09-14 2:59 AM
@Dennis Röbisch was the problem only with the hardware ? or software also ? because I am also facing the same error.

- « Previous
- Next »