cancel
Showing results for 
Search instead for 
Did you mean: 

measure power consumption of STM32F769I-DISCO

aben118
Associate II

i want to measure the power consumption of my stm32f769 discovery board, while its runs a simple NN model. Is there any way to do it using the STMCubeMX? or do i need to get a X-NUCLEO-LPM01A power shield? If so, would that be compatible with the STM32F769I-DISCO? @Stephanie Low @FBL 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Jaroslav JANOS
ST Employee

Hi @aben118,

yes, you need the X-NUCLEO-LPM01A power shield, which is compatible thanks to the Arduino connector. Then, you can monitor power with STM32CubeMonitor-Power (link).

BR,
Jaroslav

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.