cancel
Showing results for 
Search instead for 
Did you mean: 

Can't get from STM32H743 (LQFP100) ADC good accuracy

moranf
Associate II

Hello,

In my project, I sample the ADCs ( ADC1 & ADC2 ) every 1 millisecond.

My ADC configuration :

  • VREF = 3V
  • FADC == 8M
  • Prescaler = divide by 8
  • 3 channels for each ADC
  • Sample time - 64.6 cycles

In order to test my ADC driver, I inject 1HZ sinus. to 1 of the ADC1 channels.

The issue is that I can't see the LSB's bits change in a natural way.

The sample results (raw data) change like this :

64,127,1024, 2048

I can't get the 50uV (3/2^16) resolution.

Please advice,

If need I can upload the IOC file or any other source.

Best regards,

Moran

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bowman32
ST Employee

Hi @moranf​ 

You can refer to application note AN2834 "How to get the best ADC accuracy in STM32 microcontrollers" with intention on section "3. ADC errors".

Bouraoui