2019-02-26 2:03 PM
I created a project for using the STM32F746 DISCOVERY board with LwIP utility (see image 1 and 2 ). As soon as the project was created i tried to build it but ended up not beeing able to do so and getting the following error(see image 3):
Hope someone can help to deal with this.
Thanks.
2019-03-06 12:25 PM
The first error says very clearly what is the problem. Maybe try actually reading it...
2019-03-06 1:50 PM
Hi piranha,
My problem is that the file is in the correct folder but i do not understand why this error is appearing. Also why there is a problem with a third party library given by Stm