cancel
Showing results for 
Search instead for 
Did you mean: 

Can sdio f_mount affect UART port?

MCięż.1
Associate

Hi!

I have a problem with the simultaneous use of an SD card (with SDIO) and the uart port with GSM module connected. The SD card works flawlessly all the time. Communication with the GSM module is very unstable when I use the SD card - using the f_mout function destabilizes the work of uart. GSM module work perfect without SD card mounted. What could be the reason for this?

I tested the DMA interrupt uart: the result was always the same: unstable operation of the GSM modem.

Hardware platform: STM32f429 discovery and SIM800L module

Software: CubeMX + HAL

Thank you very much

Regards

Maciek

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0