cancel
Showing results for 
Search instead for 
Did you mean: 

CAN on STM32F429-DISCO board

Vaclav Zajic
Associate II
Posted on March 25, 2018 at 16:45

Hello, I have question about CAN on STM32F429-DISCO board.

I found that CAN1 is shared with display control and CAN2 with on-chip debugger. In comments for this video (

/external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D4fYoXGiIdDs

) they recommend to disconnect C53 in order for CAN2 to work. In one discussion forum I found that it will be then possible to upload program via ST-link but it will not possible to debug. Is it correct? Thanks, Vaclav

null
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
T J
Lead
Posted on March 25, 2018 at 17:11

try it ...

don't forget to pull up the Rxpin if here is no line driver.

otherwse the processor will not progress beyond InitCAN

Posted on March 26, 2018 at 16:28

Hello, I tried to remove C53 and pull upthe Rx pin via 10k resistor but it still does not work. Vaclav

Posted on March 27, 2018 at 01:41

I guess you have to do what I did.

I bought a CanDo unit from UK and started it transmitting every second, then I worked on the receiver first.

then I up'd the transmission to every 10mS, it worked like a dream at 250KHz.

then I worked on the transmitter.

It may be too difficult on that board, try a nucleo board, well recommended.

(I make my own boards)

Posted on April 24, 2018 at 14:16

This answer is very help for me. I appreciate to you, sincerely.