2020-02-07 11:05 AM
Dear friends,
I get a silly error " No such file or directory " in Keil IDE while I've already added the file path to include path directory of the compiler.
This error happens only when I add lwIP source files to my project.
And what's surprising is when I remove the path in include code, the error is gone. For example, when it is written #include "lwip/opt.h" , the compiler take this line as error but I remove "lwip\" from it and write #include "opt.h" there is no problem.
Can anyone help me with this problem?
2020-02-07 11:45 AM
Stop specifying the full path in the "Include Paths". Currently you have it looking for ...\src\include\lwip\lwip\opt.h
2020-02-07 12:19 PM
Thanks for your quick reply.
The error is gone now. But I face a new error which says " error while writing browse file: No space left on device "
Could you tell me what this means?
2020-02-07 12:46 PM
The hard drive or temp directory is full? Do you have a small SSD or System Volume?
2020-02-08 2:37 AM
Yes, there is only 425KB left. Is it just because of small volume I have?