cancel
Showing results for 
Search instead for 
Did you mean: 

Can I set different Rp value on 2 CC pins by STM32 PD-PHY?

fenixzhang
Associate

I want to use STM32 PD-PHY to enable Debug Access Mode (DAM), so I need to connect both CC1 and CC2 and set different Rp values. For example apply Rp - 3A on CC1 and Rp - 1.5A on CC2.

Is it possible to do that with STM32?

If so, what family of STM32 can do that?

 

Thanks!

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Richard O
ST Employee

Hello, concerning the Debug Access Mode (DAM), this is not supported in any STM32 as of today. I believe the first ever enquiries on this feature have only come in the last weeks. Best regards, Richard

View solution in original post

1 REPLY 1
Richard O
ST Employee

Hello, concerning the Debug Access Mode (DAM), this is not supported in any STM32 as of today. I believe the first ever enquiries on this feature have only come in the last weeks. Best regards, Richard