cancel
Showing results for 
Search instead for 
Did you mean: 

Can I receive MISRA-C compliance Report about STM32G4? I would Iike to know details of it.

GJo.1
Associate


_legacyfs_online_stmicro_images_0693W00000bl5gJQAQ.png

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

Well I think compiler has options to generate warnings based on the MISRA or other coding standard chosen in the project settings. Everytime there is a HAL update, so your build will let you check it. A "certificate" to doenload may not be the best option.

CTapp.1
Senior III

MISRA compliance requires a lot more than just running a checker over the software - full details are available in MISRA Compliance:2020. In addition, I have not yet seen a MISRA checker within a compiler that offers support for all of the MISRA guidelines.

A compliance statement for something like the HAL is also only ever going to be a part of what is needed, as its use within a project may render parts of the code (in the HAL or the application) non-compliant.

All posts are made in a personal capacity
MISRA C++ Chair
MISRA C WG Member
Director The MISRA Consortium Limited (TMCL)