cancel
Showing results for 
Search instead for 
Did you mean: 

Can I enhance the timer to 96MHz on the STM32L031 processor?

Kasper Larsen
Associate
Posted on October 27, 2017 at 14:52

I am currently in the development process of a new product and I need the timer to run at a much higher frequency than the datasheet specifies.

I have a 32MHz clock connected to the processor and I need minimum 96MHz on the timers. But only on the timers. The rest of the processor is allowed to run at 'only' 32MHz.

Does anybody know if the hardware can handle such a setup?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User
Posted on October 27, 2017 at 16:13

The idea of values given in datasheet is, that they are guaranteed by the manufacturer. There's quite a lot of things going into characterization and testing.

In other words, overclocking - in any its form - *may* work. It may work on your bench, at a limited range of temperatures, voltages. Or not. And then it may fail in the field for a bunch of reasons. Or not. And it may fail for a seemingly unrelated thing - e.g. based on state of a module neighbouring to the timer on the silicon - or in a surprising way - e.g. it counts up to 13 and then jumps to 15.

So, then the risk is entirely yours; there's no point asking here.

JW

[EDIT] Besides... the timers on STM32 (except the low power ones, which unfortunately have no specs as per max asynchronous external clock) run at the system clock or a fraction of it, so you'd need to run the whole chip at the elevated frequency, too.

View solution in original post

3 REPLIES 3
waclawek.jan
Super User
Posted on October 27, 2017 at 16:13

The idea of values given in datasheet is, that they are guaranteed by the manufacturer. There's quite a lot of things going into characterization and testing.

In other words, overclocking - in any its form - *may* work. It may work on your bench, at a limited range of temperatures, voltages. Or not. And then it may fail in the field for a bunch of reasons. Or not. And it may fail for a seemingly unrelated thing - e.g. based on state of a module neighbouring to the timer on the silicon - or in a surprising way - e.g. it counts up to 13 and then jumps to 15.

So, then the risk is entirely yours; there's no point asking here.

JW

[EDIT] Besides... the timers on STM32 (except the low power ones, which unfortunately have no specs as per max asynchronous external clock) run at the system clock or a fraction of it, so you'd need to run the whole chip at the elevated frequency, too.

Posted on October 27, 2017 at 16:37

>>

Does anybody know if the hardware can handle such a setup?

The L4 will get to 96 MHz, the L0 will not.

You can't separate the CPU clock from the APB/AHB clocks in the manner you suggest.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Kasper Larsen
Associate
Posted on October 30, 2017 at 08:00

Thank to both of you! Clive One and waclawek.jan. I just thought it was best to have turned all the stones before proceeding. 

Have a great day!

/K