cancel
Showing results for 
Search instead for 
Did you mean: 

Can I change STM32F103RB to 103RC with I2S on IAR 'KSDK-STM32-PLUS' ?

davegoodway
Associate
Posted on June 24, 2008 at 06:16

Can I change STM32F103RB to 103RC with I2S on IAR 'KSDK-STM32-PLUS' ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
davegoodway
Associate
Posted on May 17, 2011 at 12:37

I wish to purchase and use the IAR kickstart for audio development using an I2S interface, so is it Ok to make a hardware change to the PCB and remove the STM32F103RB (which I believe only supports I2C), and replace it with the STMF103RC which has the I2S/I2C interface ?

Will the IAR 'KSDK-STM32-PLUS' software still work with the different chip ?

I would be bery gratefull if sombody could advise me.

Thanks Dave.