cancel
Showing results for 
Search instead for 
Did you mean: 

Can I able to connect 40 slaves (AD7719) to Part STM32F303ZET6 using single line of SCLK & MOSI? Input Cap of Slave is 10pf.Will this SCLK & MOSI have enough drive strength to drive 40 slaves? What are the things to check here?

KJ.4
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

If you have 40 chip select in multi drop, the max speed will depend on the bus signal slew rate. If you use daisy chain, sck is the most loaded signal, and mosi to miso slave propagation delay will accumulate and clamp the max speed. Buffering delays signals too.

KJ.4
Associate III

How much speed will support if i have 40 slaves in multi drop?