cancel
Showing results for 
Search instead for 
Did you mean: 

CAN Communication Issue with the Development Board.

PO.3
Associate

Hello! I have an STM32L496ZG development board. CAN communication used to work earlier. Once after the recent update of Cube IDE , CAN communication doesn't seem to work. Is anyone facing the same issue? 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @PO.3​ ,

Please share as more details as possible to help you solve your issue.

Which firmware version are you using? You can share a screenshot, or your code.

Localize where the code hangs/stop, when the problem occurs. 

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Which board are you talking about? The NUCLEO-L496ZG ?

Perhaps go into a bit more detail about you test setup, what you're doing, and your test process.

Try going back to a version that works in your sand-box, and then perhaps diff the related code / library.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..