cancel
Showing results for 
Search instead for 
Did you mean: 

CAN Bit Dom Error

ian
Associate II
Posted on August 10, 2009 at 06:33

CAN Bit Dom Error

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
ian
Associate II
Posted on May 17, 2011 at 13:19

I am using the CAN port with version 2.0.3 of the st firmware library with the keil compiler. When I setup the CAN port it works for about 2 seconds before I get the CAN Bit Dom Error. I have tested the hardware and CAN connection will another application and these work fine.

Is anyone else having this issue and any ideas how I could resolve it.

Thanks

Ian

ian
Associate II
Posted on May 17, 2011 at 13:19

I found that I was the cause of the problem I'd started using the CAN TX pin as a output about 2 seconds after start my application.

hkumar9
Associate II
Posted on May 17, 2011 at 13:19

Hi Iam,

I am working with STM32F103RBT6 at the moment for CAN Communication. My CAN is receiving the msg and it is fine. But as I transfer the msg it showing me Bit dominant Error and I really tried all possible solution. Please help me out.

Regards

Hitesh