Posted on May 17, 2011 at 13:59Hi Christoph,I tried doing it now and I did this before as well. But still the same thing. Expecting some reply from the ST technical support as I wrote mail to them. Lets see.If you have more suggestion just let me kn...
Posted on May 17, 2011 at 13:59Hi Christoph,Thanks for the prompt reply. I am using controller with date code of 946. So is quite new one as of yours. As far as code is concern it is my application specific and I am not using any of the ST's example...
Posted on May 17, 2011 at 13:59Hi,Even I am facing problem with CAN2. Although it transmit data but not 100% efficient and the most important thing is that it does transmission without enabling the TXRQ bit of CAN2_TIxR register. Most probably there...
Posted on May 17, 2011 at 13:19Hi Iam,I am working with STM32F103RBT6 at the moment for CAN Communication. My CAN is receiving the msg and it is fine. But as I transfer the msg it showing me Bit dominant Error and I really tried all possible solutio...