cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 - Servo Board (RC Servos)

askansimon
Associate II
Posted on August 03, 2009 at 16:17

STM32 - Servo Board (RC Servos)

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
askansimon
Associate II
Posted on May 17, 2011 at 13:19

Hello Togehter,

I just make the step from AVR to powerfull STM32 and need to

controll a servo.

Timer for the STM32 are for me very confused, so my question,

has somebody already made a servo board, like this

0690X0000060MkzQAE.gif

Every 20ms a Signal with lenght from 0.9 (hard left) to 2.1ms (hard right)

Thank you very mutch.

Best Regards

Askan

askansimon
Associate II
Posted on May 17, 2011 at 13:19

Hello Togehter,

ok, here is my current code

Code:

volatile s32 myTimerCounter1 = 0;

void TIM2_IRQHandler(void) {

// Also cleared the wrong interrupt flag in the ISR

TIM_ClearFlag(TIM2, TIM_FLAG_Update);

// TIM_GetITStatus(TIM2, TIM_IT_CC1) != RESET

TIM_ClearITPendingBit(TIM2, TIM_IT_CC1); // Clear the interrupt flag

//TIM2->CCR1 = 20;

myTimerCounter1++;

}

//------

// Description : Initialize the Timer2 channel-1.

// TIM2CLK = 36 MHz, counter clock = 20 ms

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

TIM_OCInitTypeDef TIM_OCInitStructure;

TIM_TimeBaseStructure.TIM_Period = 32000; // auto reaload register

TIM_TimeBaseStructure.TIM_Prescaler = 0;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

TIM_PrescalerConfig(TIM2, 19, TIM_PSCReloadMode_Immediate);

TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing ;

TIM_OCInitStructure.TIM_OutputState = TIM_Channel_1;

TIM_OCInitStructure.TIM_Pulse = 0;

TIM_OC1Init(TIM2, &TIM_OCInitStructure);

TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Disable);

TIM_ClearFlag(TIM2, TIM_FLAG_Update);

TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

TIM_ClearFlag(TIM2, TIM_FLAG_Update);

TIM_Cmd(TIM2, ENABLE);

while (1) {

// Zusammen 1 Sekunde...

Delay(250);

LED2_OFF();

Delay(250);

LED2_ON();

Delay(250);

LED2_OFF();

Delay(250);

LED2_ON();

rprintf(''Result: %dr'', myTimerCounter1);

}

The timer runs successfully with 20ms, so I try to use OutputCompare

to generate some Signal's (PIN_X On, PIN_X Off etc.)

In Timer TIM2_IRQHandler, I set this,

Code:

TIM2->CCR1 = 20;

so the the timer should generate mutch more Interrupts,

but nothing happend.

Please help. It would be great if anybody has an idea.

Thank you very mutch & Best Regards

Askan

askansimon
Associate II
Posted on May 17, 2011 at 13:19

Hello,

I just make my first steps with STM32 Timer, I have setup a mini timer

Quote:

volatile s32 myTimerCounter = 0;

void TIM2_IRQHandler(void) {

myTimerCounter++;

}

int main(void) {

// Initalisieren, STM32_Init, GPIO, UART ...

// TIM2CLK = 32 MHz, Prescaler = 100, TIM2 counter clock = 32 KHz

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

//TIM_TimeBaseStructure.TIM_Period = 0;

TIM_TimeBaseStructure.TIM_Prescaler = 100;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

TIM_Cmd(TIM2, ENABLE);

while (1) {

Delay(250);

LED2_OFF();

Delay(250);

LED2_ON();

rprintf(''Stand2: %d\r'', myTimerCounter);

}

}

Result is:

Stand2: 0

Stand2: 0

Stand2: 0

Stand2: 0

I think there is something missing or wrong, because the handler

ist never called.

If anybody has an idea, how to solve the problem,

thank you very mutch.

Best Regard from Germany

Askan

askansimon
Associate II
Posted on May 17, 2011 at 13:19

Hello Togehter,

I try also to code the Timer without the Libary.

Code:

<BR>void TIM2_IRQHandler (void) { <BR> <BR> <BR>} <BR> <BR>int main(void) { <BR> <BR> <BR> <BR> while (1) { <BR> // Zusammen 1 Sekunde... <BR> Delay(250); <BR> LED2_OFF(); <BR> Delay(250); <BR> LED2_ON(); <BR> Delay(250); <BR> LED2_OFF(); <BR> Delay(250); <BR> LED2_ON(); <BR> <BR> static s8 toggle = 1; <BR> <BR> <BR> <BR> rprintf(''Result: %dr'', myTimerCounter1); <BR> myTimerCounter1 = 0; <BR> } <BR> <BR> <BR>

But the Result is always nearly same, with the different CCR1 there

should be a big difference.

Please help...

Thank you very mutch

Askan

[ This message was edited by: askansimon on 14-01-2010 21:03 ]

andreas2
Associate II
Posted on May 17, 2011 at 13:19

Quote:

But the Result is always nearly same, with the different CCR1 there

should be a big difference.

Why? It seems you have enabled the Update interrupt which will fire every 20 ms and apparently does so. You have no interrupts related to compare/capture channel 1 enabled, as far as I can see. Even if you had, how would changing CCR1 affect the interrupt frequency? You're not resetting the counter on compare match.

askansimon
Associate II
Posted on May 17, 2011 at 13:19

Hello,

thank you very mutch, now it's working

Quote:

void TIM2_IRQHandler (void) {

// Interrupt Flag' muß per Software gelöscht werden

myTimerCounter1++;

}

int main(void) {

// ++ Initalisieren

while (1) {

// Zusammen 1 Sekunde...

Delay(250);

LED2_OFF();

Delay(250);

LED2_ON();

Delay(250);

LED2_OFF();

Delay(250);

LED2_ON();

static s8 toggle = 1;

if (toggle) {

toggle = 0;

TIM2->CCR1 = 10;

} else {

toggle = 1;

TIM2->CCR1 = 15000;

}

rprintf(''Result: %d\r'', myTimerCounter1);

myTimerCounter1 = 0;

}

[ This message was edited by: askansimon on 14-01-2010 21:03 ]