cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone tell me if the STM32F101 and STM32F103 are interchangeable?

lee79
Associate

One of our customers has replaced an STM32F101R8 in the field with an STM32F103 and cannot get the unit to power up. My question is with the same code and the same PCB will the two processors function exactly the same?

Thanks

0 REPLIES 0