2017-04-25 9:50 PM
Hi,
CAN interface on STM32F769I is not sending data using Clock configuration 1 but CAN interface is sending data with configuration 2.
I am not able to narrow down that how the CAN interface is getting affected by Clock configuration 1.
Can you pls comment on the same?
Thank in advance
Clock Configuration 1
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 400; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 8; Clock configuration 2 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 216; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 2;2017-04-27 11:13 AM
Hi ,
I could find the CAN_Networking application from STM32Cube_FW_F7_V1.6.0.In this sample project , HSE is used as clock source.I tested this application in STM32F769I evk board and found CAN packet transmit is working fine.
I have connected the evk board to host pc using a CAN bridge module.So that I could see the CAN packet in host PC which is transmitted by
STM32F769I evk board.
But the CAN packet receive is not happening When I am trying to send the CAN packet from Host PC to
STM32F769I evk board.
But the STM32F769I evk board able to receive the CAN packet from host PC when I am using the
Clock configuration 2.
I am not really wonder by seeing this result.
Is it possible to use HSE clock source for CAN receive application?
How can I use the CAN_Networking application to test the CAN packet receiving at evk side?
2017-05-19 6:37 AM
Its got solved after correcting the BS1,BS2 and SJW values.
2018-01-07 10:23 PM
Hi jith, I am also working on the same , I am also facing the same issue that CAN is able to send with Clock 2 Configuration only. Can you please tell me the values of BS1,BS2 and SJW , which worked for you and what is the baud rate your using.Please reply ASAP.
Thanks