2009-07-19 08:22 PM
Building the firmware library
2011-05-17 04:17 AM
Hi there,
I would like to use a single file compiled library instead of adding numerous source files to my projects. Unfortunately I have problems compiling the peripheral library. Does anyone have a working sample project that outputs an .lib? I'm using the Keil uVision Toolchain. Best regards Ulli2011-05-17 04:17 AM
Hi,
There is an example inside Keil with STM32 Libraries :C:\Keil\ARM\RV31\LIB\ST\STM32F10x , you can use as reference with the new one. Cheers, STOne-32.2011-05-17 04:17 AM
Thanks,
I'll try that one. Unfortunately the support at KEIL didn't point me to that example. Thank you Ulli