2009-07-23 9:09 AM
Cannot Clear EXTI Interrupts
2011-05-17 4:17 AM
I'm having a problem that seems common on these forums but the solutions offered do not seem to work for me.
I have enabled several external interrupts that go to a membrane keypad. However, when the code runs, 4 of the external lines are always triggered and cannot be cleared. If I disable these 4 lines, the other external interrupts work fine. The lines are all pulled up and I have tried disconnecting the keypad with the same result. I have ensured that the AFIO clock is running. I have also tried disabling other ports that use the same pins but the same 4 lines are still triggered. Anyone have any thoughts on what else might cause this?2011-05-17 4:17 AM
So I stripped my program to the bone and still have issues. It seems that using the MCO interferes with configuring an external interrupt on Port D.
Furthermore, I stripped the program so that it only initializes the AFIO clock, DeInits all the GPIO, then configures the EXTI and the NVIC. Absolutely nothing is running. And I still have 2 EXTI interrupts pending that will not clear. Any thoughts at all would be greatly appreciated.2011-05-17 4:17 AM
please help :-[
i can't even get a response from tech support on this issue.2011-05-17 4:17 AM
Maybe you could provide some more clues for us - for example, do you know why two of your four lines are now working? i.e. What changed, between four not working, and two not working?
And maybe post some of the relevant code? cheers, BrianWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.