cancel
Showing results for 
Search instead for 
Did you mean: 

Building Example for Nucleo-429ZI

Hasan
Associate II

Hi, 

I am new in STM32 MCU. I have bought Nucleo F429ZI, I downloaded and installed STM32CubeIDE. I have selected a new project, then I selected some examples for Nucleo-F429ZI. The name of the project is GPIO-IOToggle. 

I made a build without making any change, but it gives me the following 4 error messages: 

Hasan_0-1700328837325.png

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Hasan 

First, sorry for the inconvenience that the faced issue created for you. 

As a temporary workaround, you can keep using the 1.13.2 version however downgrade the toolchain version to the GCC10 (For more details, take a look at this post.)

PS: The issue should be fixed with the next release in the near future.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Hasan 

First, sorry for the inconvenience that the faced issue created for you. 

As a temporary workaround, you can keep using the 1.13.2 version however downgrade the toolchain version to the GCC10 (For more details, take a look at this post.)

PS: The issue should be fixed with the next release in the near future.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Pavel A.
Super User

Another workaround - see here.