cancel
Showing results for 
Search instead for 
Did you mean: 

Bugs in STM32_USB-Host-Device_Lib_V2.1.0

pa
Associate II
Posted on December 03, 2012 at 16:53

Hi all

I've tried to create a vcp communication with my STM32F4-Discovery, but I've some problems...

[code]

Description    Resource    Path    Location    Type

'struct <anonymous>' has no member named 'ddrsel'    usb_core.c    /USB_CDC_VCP/src    line 362    C/C++ Problem

'struct <anonymous>' has no member named 'i2cifen'    usb_core.c    /USB_CDC_VCP/src    line 394    C/C++ Problem

'struct <anonymous>' has no member named 'otgutmifssel'    usb_core.c    /USB_CDC_VCP/src    line 414    C/C++ Problem

'struct <anonymous>' has no member named 'phyif'    usb_core.c    /USB_CDC_VCP/src    line 361    C/C++ Problem

'struct <anonymous>' has no member named 'ulpi_utmi_sel'    usb_core.c    /USB_CDC_VCP/src    line 359    C/C++ Problem

'USB_OTG_GREGS' has no member named 'GI2CCTL'    usb_core.c    /USB_CDC_VCP/src    line 422    C/C++ Problem

'USB_OTG_GREGS' has no member named 'GI2CCTL'    usb_core.c    /USB_CDC_VCP/src    line 427    C/C++ Problem

'USB_OTG_GREGS' has no member named 'GI2CCTL'    usb_core.c    /USB_CDC_VCP/src    line 432    C/C++ Problem

'USB_OTG_I2C_PHY' undeclared (first use in this function)    usb_core.c    /USB_CDC_VCP/src    line 392    C/C++ Problem

request for member 'b' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 423    C/C++ Problem

request for member 'b' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 424    C/C++ Problem

request for member 'b' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 425    C/C++ Problem

request for member 'b' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 426    C/C++ Problem

request for member 'b' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 431    C/C++ Problem

request for member 'd32' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 422    C/C++ Problem

request for member 'd32' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 427    C/C++ Problem

request for member 'd32' in something not a structure or union    usb_core.c    /USB_CDC_VCP/src    line 432    C/C++ Problem

unknown type name 'USB_OTG_GI2CCTL_TypeDef'    usb_core.c    /USB_CDC_VCP/src    line 326    C/C++ Problem

unknown type name 'USB_OTG_CORE_DEVICE'   usb_otg.h

 /USB_CDC_VCP/src    line 50      C/C++ Problem

unknown type name 'USB_OTG_CORE_DEVICE'   usb_otg.h

 /USB_CDC_VCP/src    line 51      C/C++ Problem

unknown type name 'USB_OTG_CORE_DEVICE'   usb_otg.h

 /USB_CDC_VCP/src    line 50      C/C++ Problem

[/code]

Is there a newer version for the stm32f4 ore what?

Best regards

Patrick

1 REPLY 1
Posted on December 03, 2012 at 18:32

Is there a newer version for the stm32f4 ore what?

 

There doesn't appear to be, but the compiler is choking on code you introduced
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..