2015-12-16 3:26 AM
Hi,
I noticed this after the latest 4.20.0 update. This is experienced on a CubeMX project creation (Keil uVision). I think, the naming for the Hard Fault ISR function is wrong in stm32fxx_it.c file. I think it should be: HardFault_Handler() instead of: HardFault_IRQHandler() Am I right? Best Regards, Emre2015-12-16 4:00 AM
Yes. You are right. It's a bug of the latest CubeMX. I suggest you to change the topic title adding a ''[Bug]'' inside it.
2015-12-16 5:33 AM
Hi cnoviello,
Thanks for the reply and showing me the way to report a bug :)2015-12-17 1:42 AM
Hi emretiryaki,
Thanks for reporting this bug. Required actions will be taken to fix it.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-04-12 5:38 AM
Dear user,
This issue is now fixed in MX 4.14. Best regards