Bug Report cubeMX 4.23 IAR code genereator
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-28 12:02 AM
Hello
I use cubeMX 4.23 and have seen that the code generator for IAR itroduces absolute paths in the *.ewp project file in the include section and for all used library source files which are used in the project.
I have seen that this behaviour happens, if the cubeMX code Generator is configured to 'Add necessary library files as reference in the toolchain project configuration file'.
The former cubeMX version (4.18) I used, did not had this problem.
kind regards, A.Bischof
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-10 7:25 AM
Bischof.Arnold
Hi Arnold,
it's normal behavior i.e: when
cubeMX code Generator is configured to 'Add necessary library files as reference in the toolchain project configuration file',the
code generated for IARuse absolute paths in the *.ewp file.
if you want to use relative path you can select the other option ( copy all used librairies or copy only the necessary library files).
Regards,
Houda