2018-06-15 11:20 AM
Hi,
I am trying to learn TFT display with touch capabilities. I am using STM32F767ZIT6 MCU, RK043FN02H-CT TFT with capacitive touch panel and AS4C4M32SA SDRAM. I imported following library from STM32F746g discovery board.
#include 'stm32746g_discovery.h'
#include 'stm32746g_discovery_lcd.h'#include 'stm32746g_discovery_sdram.h'#include 'stm32746g_discovery_ts.h'I corrected pin assignments on the files and uploaded software. I was able to turn on the LCD and initialize it. Then I could not make it display color. After few research I realize that I had FBStartAdress at 0 and then I changed to 0xC0000000. I could see flickers on the screen. Then I entered FBStartAdress = 0x20013dfc. I was getting full color. I was able to draw different shapes (circle,lines, ellipse etc) but when I displaying texts it would print properly on first two lines and then it would display randomly(refer to LCD_glitch.gif or
). Here is the code snippet I'm using.#define LCD_FRAME_BUFFER_LAYER0 ((uint32_t)0x20013dfc)BSP_LCD_Init();
BSP_LCD_LayerRgb565Init(0, LCD_FRAME_BUFFER_LAYER0);
BSP_LCD_SelectLayer(0); BSP_LCD_SetLayerVisible(0, ENABLE); BSP_LCD_Clear(LCD_COLOR_RED);int
dummy = 0;
while (1)
{BSP_LCD_SetTextColor(LCD_COLOR_GREEN);
BSP_LCD_SetBackColor(LCD_COLOR_BLUE); BSP_LCD_DisplayStringAtLine(dummy,(uint8_t*)'HELLO WORLD!!!'); HAL_Delay(500); BSP_LCD_Clear(LCD_COLOR_RED);dummy++;
if (dummy>=12) dummy =0;
}
I have set text color as green but it displays in yellow. I am not sure what is causing the glitch or why color is yellow instead of green. Please refer to stmcube32.png for pin assignment.
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 432; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Activate the Over-Drive mode
*/ if (HAL_PWREx_EnableOverDrive() != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC|RCC_PERIPHCLK_I2C4;
PeriphClkInitStruct.PLLSAI.PLLSAIN = 192; PeriphClkInitStruct.PLLSAI.PLLSAIR = 5; PeriphClkInitStruct.PLLSAI.PLLSAIQ = 2; PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV2; PeriphClkInitStruct.PLLSAIDivQ = 1; PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_4; PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_PCLK1; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}