cancel
Showing results for 
Search instead for 
Did you mean: 

BOOTING STM32F469

LucasStartTech
Associate

@STOne-32 , @Peter BENSCH@Tesla DeLorean 

HI! I have my wiring below and I wonder what is wrong with it. Hope someone can give me some help!! my BOOT0 -> LOW, PDR_ON -> HIGH, BYPASS_REG -> LOW. And I have the following connections to the ST LINK:

NRST - SWDIO - SWCLK - TRACESWO.

kicad_cropped.jpgkicad_1.jpg

1 ACCEPTED SOLUTION

Accepted Solutions

Sounds like it's not powered up

VCAP should be 1.25V at viability

NRST should be pulled high internally to 3.3V or VDD

Make sure the PIN 1 is correctly orientated, bottom left corner with readable text on the IC, don't confuse with injection relief ports. Picture of the part on the board would be instructive.

BYPASS_REG : LOW

PDR_ON : HIGH

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

10 REPLIES 10

https://community.st.com/t5/stm32-mcus-products/boot-standalone-stm32f469iit6/td-p/758301

Please see my question/response at the end

Check part orientation

Check voltage present on VCAP pin, and capacitors

Check voltage observed on NRST pin

Provide a schematic, constrained to the STM32 if that's simpler, so we can better understand what you've built.

A large, clear and in-focus picture of the board with the part in-situ will also be illustrative.

The ST-LINK expects to see a target voltage on pin 1 or 2 of the standard JTAG 20-pin connector.

 

If you're getting connectivity issues in STM32 Cube Programmer, please show that whole screen, along with error message.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
LucasStartTech
Associate

@Tesla DeLorean 

I Got this:

(I Have the same values at the pin and at the capacitor)

VCAP2 -> 360mV when I insert the probe, then it drops to 312mV.

VCAP1 -> 480mV.

NRST -> 396mV.

The total drawn read in the power supply is 0.07A.

I took closer pictures, and FYI, NRST goes from the switch (I was unsure what to do with it, so I put a switch to manipulate it.) to the ST-LINK. If any question seems odd, I apologize, this is my first time trying to design a PCB. I am a CS student and therefore I have never worked so close to the hardware beforeGND.jpgPOWER.jpgST-LINK.jpgVCAP.jpgVDA.jpg. Thank you!

 

 

 

LucasStartTech
Associate

@Tesla DeLorean 

Also... this is my debugger configuration and the error I get:

conf.jpgerror.jpg

Sounds like it's not powered up

VCAP should be 1.25V at viability

NRST should be pulled high internally to 3.3V or VDD

Make sure the PIN 1 is correctly orientated, bottom left corner with readable text on the IC, don't confuse with injection relief ports. Picture of the part on the board would be instructive.

BYPASS_REG : LOW

PDR_ON : HIGH

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

f469_pin1.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
LucasStartTech
Associate

@Tesla DeLorean I have a little concern about the pin orientation. I know the dot marks the pin1, but I have 3 dots on the MCU, and therefore I assumed the pin 1 would be on the top left, as the top being oriented in a way that I can read the name of the chip. Did I do it upside down?

See image I posted above at same time you posted this.

Picture of yours would also be instructive as to what you've built..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

> therefore I assumed the pin 1 would be on the top left, as the top being oriented in a way that I can read the name of the chip. Did I do it upside down?

You have it rotated incorrectly.

With the marking on the chip oriented normally from left to right, pin 1 is on the bottom left, as shown in the picture by @Tesla DeLorean .

If you feel a post has answered your question, please click "Accept as Solution".
LucasStartTech
Associate

Oh OMG, mine is upside down then! :face_with_tears_of_joy::face_with_tears_of_joy:

I will, solder it in the right place now. I will let you know how it goes, appreciate it!!!!