cancel
Showing results for 
Search instead for 
Did you mean: 

BOOT0 direct connection to GND?

neoirto
Associate II
Posted on November 29, 2015 at 15:58

Hi all,

I just received my new layout based on STM32F2 and I can't upload via SWD (Vlink V2).

Always the same mistake : Can't reset the core...

I checked VCAP1 & 2 at 1.2V and all SWD lines.

But perhaps I made a mistake : in older layouts, BOOT0 was pulled down by a 10K resistor, but in this new version, BOOT0 is direct to GND.

Is it a problem?

Thanks in advance ;)
2 REPLIES 2
Posted on November 29, 2015 at 18:00

Is it a problem?

Well it will clearly make it difficult to do any other signs of life testing.

Do you have NRST connected to your debug interface? What is the logic state of this pin?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
neoirto
Associate II
Posted on November 29, 2015 at 18:16

Thanks Clive!

Using the internal pull up on NRST, I didn't connect this pin.

I modified BOOT0 pin to add a 17,5K resistor. Will it be enough?

(I checked : it was possible to connect to STM32 with ST-LINK utility with HOT PLUG mode).

Tx again!!