cancel
Showing results for 
Search instead for 
Did you mean: 

Boot standalone STM32F469IIT6

LucasStartTech
Associate

Hi! I am new in electronics, but I am trying to design my PCB using STM32F469IIT6. I did a similar project before using a simple atmega168, but the STM32 seems way more complex. I wonder what the minimum of hardware connection is I need to be able to BOOT or even detect the target using my ST-LINK. Right now, I powered all VDD pins and VDDA pins, as well connected all the GND pins. I set up pins 137-SWCLK and 128-SWDIO in my IDE, connected the ST-LINK, but it does not find the target. I wish someone could give me a help.

 

Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

@LucasStartTech And please don't try any of these ST-Links in colourful tin cans, because they are all fakes and don’t get recognized by the STM32CubeIDE. Instead, use an original ST-Link from a trustworthy retailer (i.e. not Alibaba or similar) so that the connection can be established.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
STOne-32
ST Employee

Dear @LucasStartTech ,

 

Welcome in our Community , Herr is a link for the minimum hardware setup required for STM32F4 series : https://www.st.com/resource/en/application_note/an4488-getting-started-with-stm32f4xxxx-mcu-hardware-development-stmicroelectronics.pdf

 And below for F469 MCU :

IMG_1053.jpeg

To better help , if you can provide schematics around all power and dedicated pins in particular PDR_On, Bypass_Reg and VCAPxx pins .

let us know ,

Cheers,

STOne-32

Peter BENSCH
ST Employee

@LucasStartTech And please don't try any of these ST-Links in colourful tin cans, because they are all fakes and don’t get recognized by the STM32CubeIDE. Instead, use an original ST-Link from a trustworthy retailer (i.e. not Alibaba or similar) so that the connection can be established.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Check part orientation

Check voltage present on VCAP pin, and capacitors

Check voltage observed on NRST pin

Provide a schematic, constrained to the STM32 if that's simpler, so we can better understand what you've built.

A large, clear and in-focus picture of the board with the part in-situ will also be illustrative.

The ST-LINK expects to see a target voltage on pin 1 or 2 of the standard JTAG 20-pin connector.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi! I've been following the diagrams, they really help! I bought an adapter, where I then soldered the MCU to be able to kind of work in the breadboard. I wired the pins in the diagram, but the ST-link did not find the target. I also got another ST-LINK as Peter suggested, and I thinking in manufacture one version, for I am wondering if the distance of the capacitors from the VDD pins are one of the reasons for my constant failure. I will post the schematic I have so far. Thank you very much!

Thank you, Peter! I got both ST-LINKS, but I've only tried the cheap one. I will port the schematic and also, I will try the other ST-LINK.

 

Thank you!!

I was working on it today, and that's what I have so far...  This the first PCB I have ever designed, so I appologize for any *** wiring. Thank you again! kicad.jpgkicad_1.jpgkicad_2.jpg

Thread then went here  https://community.st.com/t5/stm32-mcus-products/booting-stm32f469/td-p/759281

Sounds like an orientation issue

f469_pin1.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..