2016-10-11 02:31 AM
Hello everybody,
I am trying to run a BLDC motor with the FOC SDK v4.2, using a STEVAL-IHM021V2 power stage and STMF32F303RE Nucleo board as MCU. I set everything up with no trouble and connect the board to MC Workbench, but when I click start the motor shivers and stops. If I use Hall sensors, I receive a Speed Feeback fault, while sensorless I get a Start-up fault. I believe they are both originated by the same issue: the low sides for U and W are always triggered simultaneously. I have revised the connections and they are not mutually connected. Did someone have the same problem? Any solutions/suggestions? Thanks in advance, Francisco #pmsm-foc-stm32f3 #stm32f303 #nucleof3032016-12-12 08:31 AM
Hi Francisco. I have similar problem usinf STEVAL-IHM034V2 and a PMSM motor with sensorless control. I solve this changing the PID parameters, but I also not able to increase the motor speed.
2016-12-13 02:45 AM
Hi
,I recommend your hardware an software setup by referring to the user manual
-Walid F-