cancel
Showing results for 
Search instead for 
Did you mean: 

Beginner Question - #ifdef -> Where do I define the data the conditional statements are switching on

tonofsteel
Associate II
Posted on November 03, 2013 at 00:56

Hello,

I have been working with the STM8S and STM32F0 Discovery boards.  One thing that I see often is the preprocessor directives and macros.  One example found in the STM32 discovery demo code is:

  &sharpifdef DEBUG

    debug();

  &sharpendif

I tried to google the topic and I get a lot more information regarding the usage of &sharpifdef and creating macros etc.  This is great but nothing quite answered my question.

But my question is do I set the DEBUG (or other &sharpifdef) directly in code by using:

&sharpdefine DEBUG

Or should this be done a different way?

I am using IAR and I can go project->options

In this window I can go to the Preprocessor tab and there is a box there called defined symbols.  Currently it is greyed out unless I choose to ''override inherited settings'' but there is a ''VECT_TAB_FLASH'' in this box.

Should I add my &sharpdefines in this box?

I get that the &sharpifdef is switching based on defines, but where should I be setting these defines.  Is the DEBUG define automatically handled by the IAR IDE and compiler? 

If it is where would I handle setting switches say for compiling to two different versions of the STM32 chip?  For example I have &sharpifdef CHIPONE and &sharpifdef CHIPTWO sections in my code.  Do I create two different projects with the same source code but setup the defines in the options box above?  Or do I include a project defines file and set all my switches in there using &sharpdefines.

#stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 03, 2013 at 22:01

You seem to be on the right track.

Generally I'll define things within the Pre-Processor settings for global setting, and ST's libraries use these a lot. From makefiles those can come in via -D command line options.

Local stuff can either come from #defines in the file, or a related .H
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..