cancel
Showing results for 
Search instead for 
Did you mean: 

back-to-back write to the same FSMC address

gordon239955
Associate

Hi,

In my design, STM32F7 MCU communicates with FPGA via FSMC bus. FPGA emulates an asynchronous NOR flash. It was noticed that when MCU does back-to-back writes (2 lines of assembly code for each write) to the same FSMC address only the last 16-bit word appears on the FSMC bus. It seems that the first few writes are optimized away. I did check the assembly code and it looks correct. Can you advise on this?

Regards

Gordon

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Perhaps write buffers, or caching?

Perhaps change the MPU configuration for the address space the FPGA lives in, so all writes reflect, and it's not treated as a memory device.

https://www.st.com/resource/en/application_note/dm00272912-managing-memory-protection-unit-in-stm32-mcus-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..