2015-08-24 02:48 AM
2015-08-24 06:46 AM
Here are some values that the mems output (before I convert it to signed int16_t):
[128] 32700 0x20000418 uint16_t [129] 32700 0x2000041A uint16_t [130] 32700 0x2000041C uint16_t [131] 32700 0x2000041E uint16_t [132] 32700 0x20000420 uint16_t [133] 32700 0x20000422 uint16_t [134] 32700 0x20000424 uint16_t [135] 32700 0x20000426 uint16_t [136] 24722 0x20000428 uint16_t [137] 32836 0x2000042A uint16_t [138] 32836 0x2000042C uint16_t [139] 32836 0x2000042E uint16_t [140] 32836 0x20000430 uint16_t [141] 32700 0x20000432 uint16_t [142] 32700 0x20000434 uint16_t [143] 14400 0x20000436 uint16_t [144] 32700 0x20000438 uint16_t [145] 32700 0x2000043A uint16_t [146] 32700 0x2000043C uint16_t [147] 32700 0x2000043E uint16_t [148] 32700 0x20000440 uint16_t [149] 29722 0x20000442 uint16_t [150] 32700 0x20000444 uint16_t [151] 32700 0x20000446 uint16_t [152] 29469 0x20000448 uint16_t [153] 32836 0x2000044A uint16_t [154] 32836 0x2000044C uint16_t [155] 32836 0x2000044E uint16_t [156] 32836 0x20000450 uint16_t [157] 16450 0x20000452 uint16_t [158] 32836 0x20000454 uint16_t [159] 32836 0x20000456 uint16_t [160] 32700 0x20000458 uint16_t [161] 32700 0x2000045A uint16_t [162] 32700 0x2000045C uint16_t [163] 32700 0x2000045E uint16_t [164] 32700 0x20000460 uint16_t [165] 30859 0x20000462 uint16_t [166] 32700 0x20000464 uint16_t [167] 32700 0x20000466 uint16_t [168] 23853 0x20000468 uint16_t [169] 32836 0x2000046A uint16_t [170] 32836 0x2000046C uint16_t [171] 32836 0x2000046E uint16_t [172] 32836 0x20000470 uint16_t [173] 32700 0x20000472 uint16_t [174] 32700 0x20000474 uint16_t [175] 6169 0x20000476 uint16_t [176] 32700 0x20000478 uint16_t [177] 32700 0x2000047A uint16_t [178] 32700 0x2000047C uint16_t [179] 32700 0x2000047E uint16_t [180] 32700 0x20000480 uint16_t [181] 32700 0x20000482 uint16_t [182] 32700 0x20000484 uint16_t [183] 32700 0x20000486 uint16_t [184] 32700 0x20000488 uint16_t [185] 32836 0x2000048A uint16_t [186] 32836 0x2000048C uint16_t [187] 32836 0x2000048E uint16_t [188] 32836 0x20000490 uint16_t [189] 32700 0x20000492 uint16_t [190] 444 0x20000494 uint16_t [191] 32836 0x20000496 uint16_t [192] 32700 0x20000498 uint16_t [193] 32700 0x2000049A uint16_t [194] 32700 0x2000049C uint16_t [195] 32700 0x2000049E uint16_t [196] 32700 0x200004A0 uint16_t [197] 16306 0x200004A2 uint16_t [198] 22325 0x200004A4 uint16_t [199] 32700 0x200004A6 uint16_t [200] 29406 0x200004A8 uint16_t [201] 32836 0x200004AA uint16_t [202] 32836 0x200004AC uint16_t [203] 32836 0x200004AE uint16_t [204] 32836 0x200004B0 uint16_t [205] 32700 0x200004B2 uint16_t [206] 32700 0x200004B4 uint16_t [207] 12756 0x200004B6 uint16_t [208] 32700 0x200004B8 uint16_t [209] 32700 0x200004BA uint16_t [210] 32700 0x200004BC uint16_t [211] 32700 0x200004BE uint16_t [212] 32700 0x200004C0 uint16_t [213] 32700 0x200004C2 uint16_t [214] 32700 0x200004C4 uint16_t [215] 32700 0x200004C6 uint16_t [216] 19291 0x200004C8 uint16_t [217] 32836 0x200004CA uint16_t [218] 32836 0x200004CC uint16_t [219] 32836 0x200004CE uint16_t [220] 32836 0x200004D0 uint16_t [221] 32700 0x200004D2 uint16_t [222] 3056 0x200004D4 uint16_t [223] 32836 0x200004D6 uint16_t [224] 32700 0x200004D8 uint16_t [225] 32700 0x200004DA uint16_t [226] 32700 0x200004DC uint16_t [227] 32700 0x200004DE uint16_t [228] 32700 0x200004E0 uint16_t [229] 32700 0x200004E2 uint16_t [230] 32700 0x200004E4 uint16_t [231] 32700 0x200004E6 uint16_t [232] 32700 0x200004E8 uint16_t [233] 32836 0x200004EA uint16_t [234] 32836 0x200004EC uint16_t [235] 32836 0x200004EE uint16_t [236] 32836 0x200004F0 uint16_t [237] 32700 0x200004F2 uint16_t [238] 32700 0x200004F4 uint16_t [239] 12388 0x200004F6 uint16_t [240] 32700 0x200004F8 uint16_t [241] 32700 0x200004FA uint16_t [242] 32700 0x200004FC uint16_t [243] 32700 0x200004FE uint16_t [244] 32700 0x20000500 uint16_t [245] 32700 0x20000502 uint16_t [246] 32700 0x20000504 uint16_t [247] 29628 0x20000506 uint16_t [248] 32138 0x20000508 uint16_t [249] 32836 0x2000050A uint16_t [250] 32836 0x2000050C uint16_t [251] 32836 0x2000050E uint16_t [252] 32836 0x20000510 uint16_t [253] 32700 0x20000512 uint16_t [254] 55933 0x20000514 uint16_t [255] 32836 0x20000516 uint16_t [256] 32700 0x20000518 uint16_t [257] 32700 0x2000051A uint16_t [258] 32700 0x2000051C uint16_t [259] 32700 0x2000051E uint16_t [260] 32700 0x20000520 uint16_t [261] 32700 0x20000522 uint16_t [262] 32700 0x20000524 uint16_t [263] 32700 0x20000526 uint16_t [264] 32700 0x20000528 uint16_t [265] 32836 0x2000052A uint16_t [266] 32836 0x2000052C uint16_t [267] 32836 0x2000052E uint16_t [268] 32836 0x20000530 uint16_t [269] 32700 0x20000532 uint16_t [270] 32700 0x20000534 uint16_t [271] 2972 0x20000536 uint16_t [272] 32700 0x20000538 uint16_t [273] 32700 0x2000053A uint16_t [274] 32700 0x2000053C uint16_t [275] 32700 0x2000053E uint16_t [276] 32700 0x20000540 uint16_t [277] 32700 0x20000542 uint16_t [278] 32700 0x20000544 uint16_t [279] 32700 0x20000546 uint16_t [280] 32700 0x20000548 uint16_t [281] 32836 0x2000054A uint16_t [282] 32836 0x2000054C uint16_t [283] 32836 0x2000054E uint16_t [284] 32836 0x20000550 uint16_t [285] 32700 0x20000552 uint16_t [286] 48055 0x20000554 uint16_t [287] 32836 0x20000556 uint16_t [288] 32700 0x20000558 uint16_t [289] 32700 0x2000055A uint16_t [290] 32700 0x2000055C uint16_t [291] 32700 0x2000055E uint16_t [292] 32700 0x20000560 uint16_t [293] 32700 0x20000562 uint16_t [294] 32700 0x20000564 uint16_t [295] 32700 0x20000566 uint16_t [296] 32700 0x20000568 uint16_t [297] 32836 0x2000056A uint16_t [298] 32836 0x2000056C uint16_t [299] 32836 0x2000056E uint16_t [300] 32836 0x20000570 uint16_t [301] 30838 0x20000572 uint16_t [302] 32700 0x20000574 uint16_t [303] 7281 0x20000576 uint16_t [304] 32700 0x20000578 uint16_t [305] 32700 0x2000057A uint16_t [306] 32700 0x2000057C uint16_t [307] 32700 0x2000057E uint16_t [308] 32700 0x20000580 uint16_t [309] 32700 0x20000582 uint16_t