2015-08-17 3:11 PM
I'm having a problem getting all the pins to show up in the generated code from STM32CubeMX. Here's what I'm seeing:
I'm generating a project using STM32CubeMx (v4.9.0) for the STM32F3348DISCOVERY board. If I generate code without making any modifications, MX_GPIO_Init() looks correct. Here are the pins assigned:/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
PA1 ------> ADC1_IN2
PA3 ------> ADC1_IN4
PB0 ------> ADC1_IN11
PB12 ------> HRTIM1_CHC1
PB14 ------> HRTIM1_CHD1
PA8 ------> HRTIM1_CHA1
PA9 ------> HRTIM1_CHA2
PA10 ------> HRTIM1_CHB1
PA11 ------> HRTIM1_CHB2
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOF_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PA0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PA1 PA3 */
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PB0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : PB12 PB14 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_14;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF13_HRTIM1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : PA8 PA9 PA10 PA11 */
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF13_HRTIM1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PB6 PB7 PB8 PB9 */
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
If I try to add a pin (HRTIM1_CHD2 to PB15), MX_GPIO_Init() is incomplete. Here's what I get:
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
PA1 ------> ADC1_IN2
PA3 ------> ADC1_IN4
PB0 ------> ADC1_IN11
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOF_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PA0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PA1 PA3 */
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PB0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : PB6 PB7 PB8 PB9 */
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
Am I missing something?
2015-08-24 5:02 AM
Hello Tristan,
Your action enables the HRTimer peripheral ( Timer D active in your case). In this case, the initialization of HRTimer relevant pins can all be found in the stm32f3xx_hal_msp.c file. This is true for all peripherals. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.