Skip to main content
Issinski.Anton
Associate III
June 20, 2018
Question

Atollic Linker Issue: Symbols not always found

  • June 20, 2018
  • 0 replies
  • 528 views
Posted on June 20, 2018 at 08:31

Using latest Atollic TrueStudio (9.0.1) for STM32H743VI. From time to time, Atollic stops linking the project saying some symbols are not found. The only work around that I found is to re-create the entire workspace and the projects in it. Cleaning projects, deleting Debug directories does not help.

This situation was found with different projects and different scenarios, such as:

 * A weak symbol (SysTick_Handler) defined in startup_stm32h743xx.s cannot be re-defined in the project's xxxx.s file. Removing (weak) definition from the

startup_stm32h743xx.s solves the problem

;

 * Defining two symbols (functions) with the same name does not generate link error. Only re-creating the worksapce and projects solves the issue;

 * Function defined in the .cpp file reported 'Not Defined' symbol by the linker. Again, only re-creating the workspace resolves the issue.

 * Modifying library's source code does not necessary results in its re-building or re-linking with the referencing executable project.

Again, the conditions and steps to reproduce each time were different, the only common I could think are:

1. Troubled symbols were located in static libraries;

2. Source code for symbols were in linked folders (not in the Atollic's project directory);

3. Missing symbols reside in the same source file;

4. Using optimisation to remove dead/unreferenced code and data;

5. Using 9.0.1 version. Did not have a chance to try with other versions. Was using direct source include instead of libs before.

Any suggestions how to clean Atolic's workspace without complete re-creating all the projects from the scratch (takes almost a day) ?

    This topic has been closed for replies.