2024-10-08 8:37 AM
Hello,
I am trying to integrate internet connectivity on the STM32F407 using an LTE modem via the PPPoS protocol(UART). I've successfully established a PPPoS (iusing Ethernet LWIP) connection and obtained the modem IP on the STM32F407. Could you please verify my PPPoS code to ensure it's sufficient for internet access on the STM32F407? My code snippet is provided below.
int LTE_pppos()
{
tcpip_init( NULL, NULL );
enableAllInitCmd();
ppp = pppos_create(&ppp_netif, ppp_output_callback, ppp_status_cb, NULL);
netif_set_default(&ppp_netif);
ppp_connect(ppp,0);
}
static void ppp_status_cb(ppp_pcb *pcb, int err_code, void *ctx)
{
struct netif *pppif = ppp_netif(pcb);
LWIP_UNUSED_ARG(ctx);
printf("GSM: ppp_status_cb: %d\r\n", err_code);
switch(err_code)
{
case PPPERR_NONE:
{
#if GSM_DEBUG
printf("GSM: status_cb: Connected\r\n");
#if PPP_IPV4_SUPPORT
printf("GSM: ipaddr = %s\r\n", ipaddr_ntoa(&pppif->ip_addr));
printf("GSM: gateway = %s\r\n", ipaddr_ntoa(&pppif->gw));
printf("GSM: netmask = %s\r\n", ipaddr_ntoa(&pppif->netmask));
#endif
if (netif_is_link_up(&ppp_netif)) {
netif_set_up(&ppp_netif);
} else {
netif_set_down(&ppp_netif);
} // Bring up the Ethernet interface with new IP
#if PPP_IPV6_SUPPORT
printf("GSM: ip6addr = %s", ip6addr_ntoa(netif_ip6_addr(pppif, 0)));
#endif
#endif
osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT);
gsm_status = GSM_STATE_CONNECTED;
osSemaphoreRelease(pppos_mutex);
break;
}
,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,
,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,output logs:
UART6 init done
GSM: Starting Modem thread
GSM: AT COMMAND: [AT..]
GSM: AT RESPONSE: [..OK..]
GSM: AT COMMAND: [ATD*99#..]
GSM: AT RESPONSE: [..CONNECT 115200..]
GSM: GSM initialized.
GSM: ppp_status_cb: 0
GSM: status_cb: Connected
GSM: ipaddr = 10.220.50.XXX
GSM: gateway = 10.64.64.XX
GSM: netmask = 255.255.255.255
GSM: LTE Init done
After successfully connecting to PPPos, I pinged Google using ICMP but did not receive a response. Below is my code snippet.
void start_ping_action() {
//get gateway IP from global net interface
ip_addr_t gw_addr = ppp_netif.ip_addr;
uint8_t gw_ip_part_1 = ip4_addr1(&gw_addr);
//check if DHCP already succeeded by checking against non 0 ip part
int ret = 0;
if(gw_ip_part_1 != 0) {
ip_addr_t target_ping_ip;
//IP_ADDR4(&target_ping_ip, 192,168,1,180);
IP_ADDR4(&target_ping_ip, 216,58,213,195); //google.com
//IP_ADDR4(&target_ping_ip, 8, 8, 8, 8); // Google's DNS
printf("Starting to ping IP: %d.%d.%d.%d.\r\n", (int)ip4_addr1(&target_ping_ip),
(int)ip4_addr2(&target_ping_ip), (int)ip4_addr3(&target_ping_ip),
(int)ip4_addr4(&target_ping_ip));
if((ret = ping_ip(target_ping_ip)) != PING_ERR_OK) {
printf("Error while sending ping: %d\r\n", ret);
}
}
//every 4 seconds, start a new ping attempt
sys_timeout(4000, start_ping_action, NULL);
}
void check_ping_result() {
ping_result_t res;
memset(&res, 0, sizeof(res));
int retcode = 0;
if((retcode = ping_ip_result(&res)) == PING_ERR_OK) {
if (res.result_code == PING_RES_ECHO_REPLY) {
printf("Good ping from %s %u ms\r\n", ipaddr_ntoa(&res.response_ip),
(unsigned) res.response_time_ms);
} else {
printf("Bad ping err %d\r\n", res.result_code);
}
} else {
//printf("No ping result available yet: %d\n", retcode);
}
sys_timeout(100, check_ping_result, NULL);
} Output logs:
IP:10.220.50.142
Starting to ping IP: 216.58.213.XXX.
Ping timed out
Bad ping err 0
Starting to ping IP: 216.58.213.XXX.
Ping timed out
Bad ping err 0
Starting to ping IP: 216.58.213.XXX.
Ping timed out
Bad ping err 0
Starting to ping IP: 216.58.213.XXX.