cancel
Showing results for 
Search instead for 
Did you mean: 

Are VREFINT and VREFBUF output the same on STM32G4?

abhijith_raj
Associate III

Moved from this post .

Hi @mƎALLEm ,
Is VREFINT and VREFBUF output same?
In documents I have seen VREFBUF can be set as 2.048, 2.5, 2.9, is that same VREFINT?

3 REPLIES 3
waclawek.jan
Super User

> Is VREFINT and VREFBUF output same?

No.
> In documents I have seen VREFBUF can be set as 2.048, 2.5, 2.9, is that same VREFINT?

No.

JW

abhijith_raj
Associate III

Hi @waclawek.jan,
Could you please mention the purpose of that VREFBUF and VREFINT?

waclawek.jan
Super User

VREFINT is a fixed nominally 1.2V internal reference, which you can measure using the ADC, and thus indirectly establish voltage of the ADC's reference (ADC reference is always the VREF+ pin). Read the Monitoring the internal voltage reference subchapter of ADC chapter in RM0440.

VREFBUF is a voltage source with selectable voltage, which can internally be connected to VREF+ pin (but if you want to do that, you must not connect an external source to VREF+, but you must connect a prescribed capacitor to VREF+ - see datasheet). Read the Voltage reference buffer (VREFBUF) chapter in RM0440.

JW