cancel
Showing results for 
Search instead for 
Did you mean: 

Any tool to help creating a USB descriptor ?

Kuikui
Associate III
Posted on September 12, 2010 at 16:34

Any tool to help creating a USB descriptor ?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
janvi2
Associate II
Posted on May 17, 2011 at 14:06

Kuikui
Associate III
Posted on May 17, 2011 at 14:06

Yes, I found this tool, but I must admit I'm a bit lost ...

I even don't manage to understand the USB description values given in the Custom HID example.

Any tutorial somewhere ?

janvi2
Associate II
Posted on May 17, 2011 at 14:06

frankfrank954
Associate II
Posted on May 17, 2011 at 14:06

Did you manage to modify the Custom_HID demo ok? I have managed to use a larger input report ok (8bytes) by increasing Report Count to 8 in usb_desc.c and increasing buffer size. The output report fails when I try and do the same thing.

I am using GenericHID vb application from 

http://www.lvr.com/hidpage.htm