cancel
Showing results for 
Search instead for 
Did you mean: 

Another USB Device Not Recognized question/situation

gary2399
Associate II
Posted on January 26, 2009 at 19:49

Another USB Device Not Recognized question/situation

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gary2399
Associate II
Posted on May 17, 2011 at 13:00

Hello,

So I am running the Mass Storage Demo and have successfully loaded it to the STM3210E-EVAL board and have been able to detect the Eval board as a mass storage device.

However, after downloading to flash onto my project board (with an STMF103RE device), the USB Device is never recognized like that on the Evaluation board. I have the USBDP signal tied high, BOOT0 and BOOT1 both tied low.

I was wondering what I need to take into account (when switching to the 64 pin RE package) to detect this device as whatever the USB device descriptor is defining it as, in this case, a mass storage device for this example. I'm assuming the microSD card interface that is on the EVAL board is not needed to still detect this as a mass storage device?

When looking within the calls in the main.c file in this example project, I thought it may have been the USB_Disconnect_Config() function in hw_config.c, where ''USB Disconnect Pin used as USB pull-up'' might have been defined as the pull up on D+, so i set the corresponding pins to enable GPIOA Pin 11, although this had no effect.

Any direction on this matter would greatly be appreciated, thank you.