cancel
Showing results for 
Search instead for 
Did you mean: 

Always end up in Launcher:startApplication(): error with getApplicationExecutable()

SAral
Associate

I have attached the complete log here..

I am trying to use the External mode with Nucle 412 board. But with the above said error.., I am unable to connect to the board at all..,

I initially reported to MATLAB, but they closed the issue stating that it is a STM32 issue., could any one please help me out here..

3 REPLIES 3
Amigo
Associate III

I assume that you have IAR Embedded Worshop installed?

ÇSütu.1
Associate II

I am also having this problem. Any solution to it?

Jtang.3
Associate

I am also having this problem with keil . Any solution to it?

MATLAB 2020b

CubeMX 6.3

STM32 MAT/TARGET 5.6

keil 5.35