cancel
Showing results for 
Search instead for 
Did you mean: 

All UARTs are functional with DMA except for LPUART

ranran
Senior II

Hello,

I manage to operate all UART/USART DMA's except for LPUART.

For some reason, only with LPUART, I fail to start DMA transaction.

Is it because it's request are from DMA2 instead of DMA1 (all UART's are connceted to DMA1, except for LPUART, which is connected to DMA2) ?

I also call __HAL_RCC_DMA2_CLK_ENABLE in init, yet it still fail to operate LPUART1.

 The LPUART is fully operational is both polling and interrupt.

Just DMA is not functional.

#define USARTx                           LPUART1
#define USARTx_CLK_ENABLE()              __HAL_RCC_LPUART1_CLK_ENABLE()
#define USARTx_RX_GPIO_CLK_ENABLE()      __HAL_RCC_GPIOB_CLK_ENABLE()
#define USARTx_TX_GPIO_CLK_ENABLE()      __HAL_RCC_GPIOB_CLK_ENABLE()
#define DMAx_CLK_ENABLE()                __HAL_RCC_DMA2_CLK_ENABLE()
 
#define USARTx_FORCE_RESET()             __HAL_RCC_LPUART1_FORCE_RESET()
#define USARTx_RELEASE_RESET()           __HAL_RCC_LPUART1_RELEASE_RESET()
 
/* Definition for USARTx Pins */
#define USARTx_TX_PIN                    GPIO_PIN_9
#define USARTx_TX_GPIO_PORT              GPIOA
#define USARTx_TX_AF                     GPIO_AF4_LPUART1
#define USARTx_RX_PIN                    GPIO_PIN_10
#define USARTx_RX_GPIO_PORT              GPIOA
#define USARTx_RX_AF                     GPIO_AF4_LPUART1
 
/* Definition for USARTx's DMA */
#define USARTx_TX_DMA_STREAM             DMA2_Stream0
#define USARTx_RX_DMA_STREAM             DMA2_Stream1
 
#define USARTx_TX_DMA_CHANNEL            DMA_REQUEST_LPUART1_TX
#define USARTx_RX_DMA_CHANNEL            DMA_REQUEST_LPUART1_RX
 
/* Definition for USARTx's NVIC */
#define USARTx_DMA_TX_IRQn               DMA2_Stream0_IRQn
#define USARTx_DMA_RX_IRQn               DMA2_Stream1_IRQn
#define USARTx_DMA_TX_IRQHandler         DMA2_Stream0_IRQHandler
#define USARTx_DMA_RX_IRQHandler         DMA2_Stream1_IRQHandler
 
/* Definition for USARTx's NVIC */
#define USARTx_IRQn                      LPUART1_IRQn
#define USARTx_IRQHandler                LPUART1_IRQHandler

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

Which mcu?

Is the LPUART fully operational in "manual" (polled) mode?

Read out and check the relevant DMA, (DMAMUX if applicable), LPUART, and GPIO registers' content.

JW

ranran
Senior II

Yes, I forgot to mention that , sorry,

The LPUART is fully operational is both polling and interrupt.

Just DMA is not functional.

Thanks