2023-10-06 04:39 AM
I configured the EXTIs for 16 inputs from PD0 to PD15, rising and falling edge, IRQ1 for PD0, IRQ2 por PD1, and so on as must be for groups 5-9 and 10-15 IRQ Handler. I debug the program with a breakpoint in each EXTI_IRQ_HANDLER and all of them are activated when I press a button. I found the behavior of the callback because of this but I do not know the cause.
Solved! Go to Solution.
2023-10-06 02:37 PM