2024-03-17 10:46 PM
I'm using the STM32G030FP6 in standby mode with WKUP2 for wakeup and the system has a backup battery. I'm facing the following issues:
2024-03-18 06:07 AM
Hi, i don't think if i can resolve your problem but did you use the PC13 GPIO on your board ?
because on the erratasheet i found this issue:
2.2.7 PC13 signal transitions disturb LSE
Description
The PC13 port toggling disturbs the LSE clock.
Workaround
None
QM
2024-03-19 10:34 AM
On my system, PC13 is not utilized (STM32G030FP6 doesn't have PC13), and during debugging, I've discovered that I can't enable the LSEON bit of the BDCP register during abnormal startup.