cancel
Showing results for 
Search instead for 
Did you mean: 

ADC simultaneous channel conversion.

siddj
Associate II
Posted on February 13, 2009 at 17:34

ADC simultaneous channel conversion.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
siddj
Associate II
Posted on May 17, 2011 at 13:02

I have PC0-IN10, PC1-IN11,PC2-IN12 connected to 3 analog inputs. All 3 port C pins can be configured for ADC 1,2,3. I was wondering if it is possible to configure 3 channels from the same adc and have them convert simultaneously?

or should I assign 3 different ADC's to the 3 analog signals, since I know i can convert data simultaneously on 3 different ADC's.

Also what formula should i use if i am just reading a voltage from 0-3.3 V?

How do I convert that value from ADC_DR register to a voltage for a specific sampling time?

Thanks for your help!