2008-10-13 8:15 PM
adc sample trigger
2011-05-17 3:47 AM
Hi all,
I am designing a buck converter using a STM30F103RBT6. I am trying to measure the mosfet current and I am wondering is possible to trigger adc to sample in the middle of a pwm pulse? mark2011-05-17 3:47 AM
Hi Mark,
I'm working on the same problem, and found out, that the best solution, would be to programm the regular ADC and the injected ADC to be triggered by a Timer. See Section 10.7 in the reference manual for this. Mostly you want to measure the current in the middle of the high and in the middle of the low phase of the PWM signal. My approch was to sync all timers and use TIM1 CC2 for regular channel trigger (middle of high phase) and TIM3 CC3 for injected trigger (middle of low phase). So much to the theory, as you can see in my thread, the triggering itself is not working. If you find a solution to this problem, I woulb be glad if you could report back here. Janosch2011-05-17 3:47 AM
> My approch was to sync all timers and use TIM1 CC2 for regular channel
trigger (middle of high phase) and TIM3 CC3 for injected trigger (middle of low phase). given the uncomfortable interface differences between regular and injected (dma vs register), maybe you could consider these options. first the ugly one: use a single timer. one channel does PWM. another channel triggers injected. you don't use register shadowing for the injection triggering so that you can change it mid period. on each ISR after injected conversion you configure the trigger value for the middle of the next half period. note that you get two ints per period. and the much nicer option: configure one timer for up/down counting with center-aligned pwm (optionally with double updates for twice the resolution). the two mid-half-period sample points now occur when the timebase is zero and maximum. so now maybe you can trigger the ADC directly from the timebase update events. (if not -I doubt it-, you could use two compare channels with constant values; you might need to synch a second timer.) > So much to the theory, as you can see in my thread, the triggering itself is not working. ST has ACIM and PMSM field-oriented motor control libs that sample synched to PWM. maybe you should take a look there.2011-05-17 3:47 AM
> you don't use register shadowing for the injection
> triggering so that you can change it mid period For me, this is (sadly) no option, as I use the shadow feature for changing my timer configuration atomar. > configure one timer for up/down counting with center-aligned pwm Nice idea > ST has ACIM and PMSM field-oriented motor control libs > that sample synched to PWM. maybe you should take a look there. I found the documentation of it, and it looks nice, but where can I find the code for the lib itself ?2011-05-17 3:47 AM
> where can I find the code for the lib itself ?
you have to talk to support and be prepared to accept a non-free license (and have patience). let me stress that I think that center-aligned pwm is a better solution.