2014-03-20 5:52 AM
Hi,
I am trying to use ADC for reading the voltage on pin A4.. I wrote an initialization method, however it get stuck in the last WHILE. Here there is the code: void ADC_Initialize(void) { ADC_InitTypeDef ADC_InitStructure={}; GPIO_InitTypeDef GPIO_InitStructure={}; /* Enable GPIOA clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Configure PA.4 (ADC Channel 4) in analog mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Enable ADC1 clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); /* ADC1 configuration */ ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* Wait until the ADC1 is ready */ while (ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET); } Here some register values read in debug Status register SR=256, Control registers CR1=0 and CR2=1. The problem is the bit ADONS (bit 6 of SR) that is never set.. and i get stuck inside the while... Any idea why this happens? #adc #stm32l #discovery2014-03-20 6:16 AM
I actually found the error...my code uses the MSI clock..... but for making the ADC work, the HSI clock must be enabled anyway...